This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A1601 spice model not working in TINA-TI

Other Parts Discussed in Thread: TINA-TI, TPS7A47, UCC27714

It seems the spice model available on the TI-product-page will not import correctly as Macro into TINA_TI, V9 (Version 9.3.50.40 SF-TI). It is also not availble as a preinstalled component in the library.

I get the following error: "Invalid device: $CDNENCSTART. Line #38" when the TINA is trying to parse the .lib file

If there is a way to simulate with this circuit in TINA-TI I would be most greatful.

I get same error for TPS7A1650

 

BR

/John