Other Parts Discussed in Thread: UC1901, TINA-TI, UCC28C41, UCC28C45
Hi,
Can I get the spice model for UC1901?
I am not able to use the Pspice model which is available in Ti website.
I simuate my circuit using LtSpice.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shihab,
We do not support LTSpice and can not provide a model for this tool. You can get an unencrypted model for this part if you want, but you will have to work with your local Field Applications engineer. You might also need an NDA with TI.
Alternately, you could use the TINA-TI model in the product folder: http://www.ti.com/product/uc1901#simulationmodels. TINA-TI is a free simulator that TI provides and can be downloaded here: http://www.ti.com/tool/tina-ti.
Best regards,
Hi Shahib,
Currently, we do not have a model available for UCC28C45, but we do have a TINA-TI model available for UCC28C41 which has a lower startup voltage. Can you use this one instead?
http://www.ti.com/product/ucc28c41#simulationmodels
Best regards,
Hello Nikhil,
I am doing simulation with UC1901 , the unconnected pins of the circuit are creating error, like external clock, NC,NC1 and status, uis there any solution ? can it be grounded ?
Regards
Prasanna Sinthaje
Hi all,
I am having some troubles simulating with Orcad 10.5 the transient and average model.
For all simulations the PSpici A/D gives this errors:
.SUBCKT UC1901 CT EXTCLK NC DRIVERB DRIVERA NC1 GND VIN STATUS COMP INV NINV VREF RT
* Oscillator *
$CDNENCSTART
$
ERROR -- Invalid device in subcircuit
eee8c5c7a2bc4b01f045f303678664e7916da0bae22e8cb0bba041dd67c69ce448ea70148a9ac1670c8926c1ac5057c8ccfcd77bf87ca9dc0b84dea08e3fb82d
--------------------------------------------------------------------------------------------------------------------------------$
**** EXPANSION OF SUBCIRCUIT X_U1 ****
X_U1.$CDNENCSTART
-$
ERROR -- Invalid device
Any advice? Thanks in advance,
Andrés.
Hi Andres
The model from the web is encrypted and will work in versions 15.7 and above alone. you will need an unencrypted model which you can request from your field application engineer.
Regards
Ranjani