Hello,
I'm trying to design a circuit with the TPS40170. I used Webench with my requirements, 22-36Vin, 13Vout. Most of the time it will only draw 2A, but it will have occasional pulses at 13A for 50ms. If I put the load at 13A for worst case, the TPS40170 doesn't show up as an option. I thought the TPS40170 is capable of 20A, is that correct? If so, why would it not show up in Webench as an option? If I lower the load to 10A, it does show up. Is this the right device for my requirements, or should I use something else. The reason I wanted to use the TPS40170 is that it seems to be a good device for the rest of my loads.
Thanks,
J