Dear forum members,
I am trying to use Webench to simulate a 24Vdc to 12Vdc converter using the LM3150 but without success.
The Startup simulation shows the output voltage rising to just 0.4V and then falling back to 0V within 700uS, never reaching 12V.
The Load Transient simulation from 0.01 - 6.00 amps produces unuseable results.
I would also like to simulate a zero load condition.
Any help would be greatly appreciated.
Aaron
Configuration for LM3150
Vin Min = 23V
Vin Max = 25V
Vout = 12V
Iout = 6A
Amb. Temp =40