This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi mates,
When I ran TPS54528 swticherpro simulation, it got some problems about the bode plot.
Spec: Vin=12V, Vout=3.3V, Iout,max=4A
Schematic
If yes, why bode plot can not be measured through switcherpro? Does it relate to TPS54528's control topology, DCAP2?
Thanks
Grace
Hi Grace,
Yes. It is related to the DCAP2 topology. Please refer to Table 1 of the datasheet as well. The recommended values in the datasheet ensure that the system is stable.
Regards,
Gerold