Dear All, I need to calculate the differential low-pass filter with a single output, the example schema:
I calculated the values of the components in the circuit with FilterPro:
The problem is that the calculation in Filterpro I pointed Gain=1(2Vrms to 2Vrms), but the simulator shows a gain=2(2Vrms to 4Vrms) - probably because I had hoped to Filterpro "Fully Differential LPF", and gathered in the simulator "Diff with single out".
How do I calculate the "Differential LPF with single out"? Theoretically there is such a description in the patent , but I want to do calculations with the help of the program - is automated.
Warmest regards
Vitalij