This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

W- bench tool functioning

Other Parts Discussed in Thread: LM5118, LM25118, TPS40210, LM5122-Q1, TPS40210-Q1, LM5122

Hi 

I have to use a synchronous dc-dc converter module with specifications 

Min i/p V - 6V

Max i/p V- 24V

Output Voltage - 12V 

Nominal input voltage - 12 V

Output current - 3A

I had tried to simulate the same using W-bench  s/w  , to check the efficiency at diff - diff input voltages level , but  simulation not completed , most of the time error message , this component has nor range appears or in other case  if i put min volateg as 9 and max as 24 then results appear and  if i change input like 6 - 12 then message appears to select some other components . Please resolve my query and  if my procedure is wrong somewhere then guide about that .