Other Parts Discussed in Thread: LM3414HV
I have a little problem with a circuit that I have inherited. I have included a .zip with two jpg's that outline the problem precisely. But it boils down to the fact that when the LM3414HV is "shut down" with a low on the DIM pin, the thing still draws about 6uA through the LEDs, which is way too much for my application. I am not really a power guy, and more of a control designer, so I am a little lost on this one, and I need to get a prototype out reasonably soon. I am open to workarounds or different topologies, as this is going to be a high volume product, with 6 to 12 circuits per unit, and unit volumes around 100K/yr by 2015.
HELP!!! ;)
(feel free to contact me.)
thanks,
-Dave