Other Parts Discussed in Thread: TPS54218, TINA-TI, LM5009
John recommend me to use TPS54218 as a substitute simulation for TPs57112Q1.
This design is just to step down 5V to 3.3V/500mA.
problem No.1: if I use the battery as input voltage 5V start to calculate DC nodal voltage, it results a warning, operating point not be found, related mistake on switching controller (Component: U1.X_U8_U296.D_D11). I could go around this problem by replacing battery with voltage generator and defining a voltage piecewise linear.
refer the schmatics (attached file)
Problem2 No. 2 (main problem): I like to do small signal analysis. I have to add a voltage generator (sinusoidal ) at feed back loop to calculate the ac transfer function.
response from Tina: two signals source can not be used (because there is one already on input side & second in feed back loop).
As suggested there is a slope compensation therefore simple/ideal condition is not enough for loop compensation.
Perhaps I have to buy Tina-Ti instead of free version from designsoft.