Hi,
I am attempting to model a spark gap to be used as the load on the output circuit of a high voltage ignition module that I would like to simulate. There are a few spice models available on the internet, the most promising of which I have imported into a TINA macro. No error were reported during the import however the model (which appears to be quite strait forward) does not converge. I suspect that there are some spice syntax differences causing the problem but despite reading lots of posts on this forum I have not been able to find an issue. any help you can provide in identifying the problem would be greatly appreciated. I have attached the netlist.