Hello again!
I notice that TPS40054's data sheet says the following:
Duty Cycle Max (fsw < 500KHz): 85% .. 94%
Duty Cycle Max (fsw > 500KHz): 80%
SwitcherPro only allows max. 80% even if I use 325KHz switching frequency?
Is it okay?
BR,
Krisztian