Other Parts Discussed in Thread: TPS40210
Hi All,
I have been using the online version of Switcher Pro for a TPS40210 and created designs with the following inputs
Vin min = 11
Vin max = 14
Vout = 50V
Iout = 2A
In the past this design was created with no problems but there was a warning that the current through the output cap exceeded the recomended value. I was then able to go to the output cap and select a different cap and by following the recomended number of caps and any warnings, the design would be created without any warnings.
In version 3.4, I am unable to get to even a design with warnings.
Should I take this to mean that some major problem was found that invalidates the design I was working on from the previous version of Switcher Pro?
If I open up the design done in the previous version of switcher pro, version 3.4 does pick up on the incorrect spec for the CSD1623Q3 which had a Vds of 60V previously but is actually 25V. However the other parts of the design don't raise any issues.
I know that you aren't aiming to create a fool proof design suite that will replace the power supply designer but I am pretty new to power supply design so I am looking to the tool to guide my design process.
Please let me know if there is more info I can provide to help understand the question.
Finally, just want to say that the Switcher Pro is a FANTASTIC tool and it certainly help heaps of people with their designs AND sell TI hardware at the same time.
cheers
Peter