Other Parts Discussed in Thread: TPS63000, TPS63010
I'm debugging one of my last boards and I wanted to double check with you guys that what I have is correct. I am using the TPS63000 and I want to change the output voltage from 3.0V down to 1.8V by using a FET to bring in a 374k resistor in parallel.
There is a divider on the feedback pin (FB) and I am using a 887k and a 340k divider. Then once the FET is turned on I will have 374k that is connected to the midpoint of the divider.
Is this easy to simulate with Switcher Pro?
Thanks for the assistance.
-Henk