Other Parts Discussed in Thread: TPS54140, TPS40140, TPS54160
When we designed the application circuit with the same conditions(VIN=10V-16V, VO=5V, IOmax=1A, Fsw=2.2MHz) on both TPS40140 and TPS40160, We had a different result. In case of TPS54160, the following commnt was displayed. but,no comment for TPS54140. Both devices should have the same characteristics regarding minimum controllable On time. Why does TPS54160 only has the following comment?
Duty cycle is too low for the device in this situation. Calculated on time is below the 'Minimum Controllable On Time'of the device! Use the analysis tab to view the calculated on time. This device has a 'Minimum Controllable On Time' of 130ns.