This version still with bugs for TPS54160 because the "loop" page still showing a phase and gain margin graphics with different results after starting " what if" analysis.
If the software calculates a compensation circuit with for example 60 degrees of phase margin, and then if you activate " what if" analysis without changing anything and then just press "calculate" button to just verify if the result is correct (for the same componentes values that the software calculated before), it will change to 42 degrees!
I already posted the same problem before and TI told me that this should be fixed
Does anyone knows which results is reliable?
I really need to design with TPS54160 for high volume production but this software seems to be just a loosing of time for engineers.