This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Minimum on-time of TPS40210

Other Parts Discussed in Thread: TPS40210

I'm designing a boost conveter based on the TPS40210.

Input voltage is 48V 5% and the output voltage is 67V.

SwitcherPro is telling me that at 700kHz switching frequency the minimum on-time requirement is violated because it needs to be more than 400ns.

The datasheet actually specifies that when Vdd is 30V (as it is in my case) the minimum on-time requirement is 200ns in worst case.

Is SwitcherPro consistent with the datasheet?