This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The result of SwitcherPro is different with my calculation

Hi, gentleman :

I tried to use SwitcherPro to calculate my design, but I found the result is different with my calculation

1. The output capacitance is 58uF , but SwitchPro is 470uF

2. The power inductor L1 is 8.2uH, but SwitchPro is 1uH

I recognize the parameters are different with mine, but I believe if I set these parameters as the same as SwitcherPro, these results are different still. Can you give me a tip ?

BR

Stone