This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54332 suspicious peak at fsw/2

Other Parts Discussed in Thread: TPS54332

I'll copy this here since it's more of a switcherpro issue than smps design issue. 

I made a 4.3V -> 3.3v smps design with TPS54332 for 0.5A load and 4.7uH ind, 22uF ceramic cap.

Switcherpro (correctly) shows the fsw/2 peak with inadequate slope compensation as shown in Ridley's and Sheenan's papers on CMC modeling. However the Q of the peak seems to be calculated differently from the published papers.  With 4.7uH the peak is severe. Going to 10uH inductor the peak practically disappears which seems a bit unlikely relationship to the double pole Q. I played a bit with the what if scenarios and there peak seems to go from very large at 6uH to neglible at 9uH.

In Sheehan's Current-mode modeling paper the inductor inductor size is just a denominator in the Q equation the wouldn't peak jump like that with halving the inductor size.

Is the switcherpro model correct wrt network analyzer?