Other Parts Discussed in Thread: TPS54160
I found a bug on TPS54160 compensation network calculation.
For a same identical situation, Switcher Pro calculates and shows two differents results for Gain and Phase Margin.
For example, if you start a new advanced design for TPS54160 with this parameters:
Vin min = 8V
Vin max = 36V
Vout = 5V
Iout max =1.5A
Iout min = 0.1mA
Vo ripple = 100mV
frequency : 600kHz
soft start: 100us
Gain Margin: 20
Phase Margin: 60
Transient Step Voltage: 5%
Swicher Pro will calculate:
C7=6.8p
C6=1200p
R3=44,2k
R1=10k
Without modifying anything, If you just take a look on "loop" tab, you will still seing a calculated Phase Margin of 60 Deg and a Gain Margin of -18dB.
But, if you just press "Calculate" button not changing any parameter, Switcher pro will calculate a new Gain Margin of -19db and a Phase Margin of 41 Deg with the same network components calculated before!!!
Does anyone knows wich result is reliable?
Best Regards,
Jorge