Other Parts Discussed in Thread: TPS54331
I am using a TPS54331 switcher and am seeing noise in the form of regularly spaced (1 us), 100MHz damped sinusoidal transients of about 500 us in duration on the output. I used switcher pro to design the circuit which lists the cross over frequency as 1.7KHz and the phase margin at 86 degrees. To isolate the problem I built another board, populating only the switcher circuit. Whenever power is applied to the input of the switcher I see the transients.
Do you have any suggestions about what might be causing the transients?
Thanks