This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54383 - Why can't I change the compensation resistor?

Other Parts Discussed in Thread: TPS54383

When I specify the following settings for a TPS54383, the SwitcherPro model doesn't show me the value of the compensation resistor of the 2nd output. A symbol of a resistor is drawn, but it has no reference designator.

It seems also not possible to edit/change the value. Is it a bug in the model?

Input voltage: 4.75...12.6V

Output1: 3.3V 2A

Output2: 1.2V 2A

note: when I swap the outputs, the problem occurs with the compensation resistor of the first output...