Other Parts Discussed in Thread: TPS40057
Hi! I have built a DC/DC converter with a TPS40057 based on my design (ID: 38122). Unfortunatelly it is not working, it outputs about 5V ~ 8V instead of 12V, and it is swinging.
I have redesigned the compensation components according to the current data sheet of the device. Now it is working (outputs 11.98V), but sometimes the output goes bellow to 8-9V for 10-20 seconds.
The load typically drains 1.5A. I also had to add a snubber, because it didn't get wokring until I have added. Peaks were very big (45-50V). According to the application note on how to design a snubber, i have found the value of parasitic cap. and inductance of the borad.
The second problem is that the application note says that i have to add Cpara * 3 or greater value of cap. to enough reduction to the peaks. The design has about 310 pF parasitic capacitance. If I add a 910pF cap. the peaks are reduced by 5-7V, but if I add an 1nF cap. the oscillation won't start (I see 4-5V DC with my scope on SW node). It is bigger, but where is the problem? Why the voltage isn't 12V at the output with the original design.
Please give me some suggestions!
Design ID: 38122, application note: SLVA255.
Note: I use 1uF caps for C3 and C4 and Si4840BDY (i can't get Si4840DY because Vishay says that this FET is obsolote and replaced with Si4840BDY - very very similar).
Thanks for your help!