I used Switcher Pro and the TPS40210 switcher to design a circuit. I noticed the foot note indicating the " Duty cycle is too low for the device in this situation. Calculated on time is below the minimum controlllable on time of the device! " From the analysis data the design has a switching freq of 700 khz and the device has a minimum controllable on time of 400ns.
What do I need to do to increase the duty cycle?
Thank you,