Other Parts Discussed in Thread: TPS5420
When I design a circuit using the TPS5420, I get C1 with an "OPEN" value and C9 with a value of 3.3uFd. When I look at the Layout view, it tells me I typically need a 10uFd bypass capacitor. In the spec sheet, it says I need bypass capacitance and sometimes also need a bulk input capacitor. My question is, do I need to add 10uFd input bypass capacitance? Is the recommended 3.3uFd considered the bulk or the bypass capacitor? What is the total required for bulk and bypass?
Thanks - Barney