Other Parts Discussed in Thread: TPS54917
if I make a design 3.0V to 0.9V 3A using TPS54917 I get a warning that minimum ontime is violated. This happes as the default frequency is 1.6MHz. but there is no easy way to change the frequency to a lower value. the only way I found is to make a new design using the advanced tab and there select a new frequency.
Please add a function to allow a customer to change the frequency in an existing design. especially as the software already gave a warning about minimum ontime violation.