Other Parts Discussed in Thread: TPS54331, TPS54233, TPS51116
I am using the switcher pro tool but I cannot get the TPS54331 converter to build a circuit from 24V downto 1.2V @ 3 Amps without any errors.
I keep getting "Duty cycle is too low for the device in this situation. Calculated on time is below the 'Minimum Controllable On Time'of the device! Use the analysis tab to view the calculated on time. This device has a 'Minimum Controllable On Time' of 160ns."
Will this part work for these voltages as the spec states?