Other Parts Discussed in Thread: TPS54610
When I use the Switcher Pro utiity, the VBIAS capacitor is always 0.01uF. According to the datasheet a 0.1uF to 1.0uF capacitor should be used.
Is this a bug ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS54610
When I use the Switcher Pro utiity, the VBIAS capacitor is always 0.01uF. According to the datasheet a 0.1uF to 1.0uF capacitor should be used.
Is this a bug ?
Typically these parts are set by the application engineers to be a fixed value. If it's not matching the datasheet then it is possible that there is a bug in the value. Each device has it's own specification. On which device did you see the discrepancy?