Other Parts Discussed in Thread: TPS5430
On TPS5430 application circuitry, The calculated SBD(D1) dissipation is showed on STRESS screen. But that power dissipation is not correct, I think.
My conditions for the application are; VIN=11V-13V(typ=12V), VO=3.3V, IO=3A. On the default application created based on that conditions, D1(catch diode)'s dissiopation was 202mW at 2.59A RMS current. It means Vf of D1 is about 80mV. too low. The calculation should be corrected, I think.