This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cadsoft Eagle import issue

Hi,

I was very surprised to see that you managed to support Cadsoft Eagle 6.4 as well.

But only the schematic seems to work as expected (more or less, GND signals, power source and load reported an error cause they were not connected)

But now I tried to generate the .brd file out of the schematic. Then I get just some points but nothing usable. Hope at least should work? This would save me several hours on each design!!!

Also the provided link is not working:

For additional information, please visit this site:
http://www.accelerated-designs.com/help/Eagle_import_BRD_SCH.html

Would be nice to get som help on this.

Kind regards, Chris