Hi,
in the Project Summary page, I do not have the option to Export. Only Design Document,share the design and Copy this design is present as shown below. Please let me know how the design can be exported to CAD.
Thanks,
Elizabeth
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Elizabeth,
Can you please let us know which device you were using?
Thanks,
Jeff
Dear Sir
I have the same problem - I want 4.5-5.5Vin, 9V@0.9A out, max efficiency.
Webench offers me designs using TPS43060, TPS43061 , 96% efficient (great), but no export :-(
On the same page LM5122 and most others do have CAD export. (TPS55330 doesn't)
Is there any chance of adding CAD export to the 4306x chips?
Many thanks
--David
Hello,
We should have the Export enabled for the TPS43060, TPS43061, and TPS55330 by Jan 29th.
Thanks,
Surinder
Hello David.
As promised, the schematic export for the requested TPS devices are enabled online. You can reload the created designs from My Designs/Projects list and export the schematics.
Hi,
Thanks for the support. It was found at that time that CAD export option was shown only for certain criteria. I was searching for Vin = 8V to 12 V, Current rating of 3A. Schematics for certain ICs were shown but Export to CAD option was not there.
Now I am able to get a few ICs with the export option for the required criteria. Thank you all for the support.
Thanks,
Elizabeth
David,
I am glad that it works for you.
Thanks for using WEBENCH tools.
Regards,
Surinder