There is not a .tsm file for the part CSD13303W1015 mosfet. This pspice model available for download contains a .lib file for pspice and an .olb file which is the symbol for Capture. I am trying to generate a macro in TiNA such that I can simulate using this MOSFET. However, the model is encrypted and is causing issues. Can encrypted .lib files be used to generate a new macro ? the new macro wizard freezes after I select a symbol, the netlist shows (which is encrypted) and I click next. Any thoughts or ways around this issue ? Thank you for your time.