Other Parts Discussed in Thread: TPS62177
Hi,
I'll use TPS62177 in a project. I'm using the Webench tool to check BOM and features etc.
I'd like to export the schematic to Cadsoft Eagle Cad 6.4 but there is an error:
ERROR: Exception occured while looking for CADExport error messages. Could not find file 'Z:\39\47\3947213\9\Eagle\2014-01-14_07-40-21\readme.txt'.
I saw also the error:
ERROR: Error - Incorrect pin mapping for component TPS62177DQCR looking for pin 24..
Is it possible to fix that?
Best regards, Elias