Fault 1) As far as I can see, the polarity on the bottom-left winding on the transformer has the wrong polarization. When current on the main winding, the detection feedback should respond positive. (This is what the samples in the datasheet does)
Fault 2) Symbol for adjustable zener diode (I assume this is the component missing here) is just a big rectangular blob.