Other Parts Discussed in Thread: TPS55340
Hi,
With a Webench solution using the TPS55340 in boost configuration with a Vin range of 12 - 24VDC (18V nom.) and 36V output @ 500ma. I assume the output impedance is determined mostly by the output capacitor. How could I further increase the output impedance to aprox. 60K @ 1KHz? Simply adding a series inductor to the output would appear to require a large 6-7H inductor.
The reason for the high impedance is so to supply a network with a DC voltage on which devices can inject a low frequency (500Hz - 20KHz) AC signal.
Regards,
Rob