Other Parts Discussed in Thread: TPA3111D1, TINA-TI
Hi. Please help find an amp PSPICE model for Altium Designer.
Maybe someone has a library for Altium with this amp?
Help please, urgently need to simulate a device with this amp!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Petr,
I am not 100% clear what you asked for.
Do you ask for:
1. An amplifier model that can be used together with TPA3111? or
2. TPA3111 pspice model?
If this is the second one, we already have have TPA3111 pspice model located on
TPA3111 product folder: http://www.ti.com/product/tpa3111d1
You can open the .lib file contained within TPA3111D1 TINA-TI Spice Model (Rev. A)
and you can try to import it into Altium Designer. If it gives you error, let us know, but usually
it should work with no problem.
Herman
Hello,
I'm having the same problem. I'm trying to open the .LIB in OrCAD but it's encrypted.
Thank You
Valentin
Sorry guys,
I didn't realize that the even the .LIB for TINA-TI (the one I gave you the link) is encrypted.
I thought it was just missing .LIB for orCAD but it had unencrypted .LIB for TINA-TI.
I will ask if we can unencrypt the model AND put it on the web (not 100% sure). But if we
can't, the best perhaps we can do it to provide .LIB encrypted that works in OrCad/Pspice (not 100% sure
yet for the Altium case).