Other Parts Discussed in Thread: LM3671, TINA-TI
The reference design and spice symbol is only for 2.5V output.
Not a realistic simulation for other voltages available.
It's a joke, or is the LM3671 at EOL.
Rolf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Rolf,
When I changed the circuit to use feedback resistors and a different inductor, I got the model to simulate for 3.3V out correctly. However, for many other output voltages, I did not get the proper simulation.
I am investigating the model currently. Thanks for pointing this out. This part is a little confusing since it is available in many fixed voltage versions as well as the adjustable version.
I'll let you know what I find out.
Britt
Britt,
that's right. But when I set the input voltage to 5V, I get 4.7V output voltage instead of 3.3V.
That's the problem.
Rolf
Rolf,
Try this one. I believe it is correct now for the adjustable version.
Britt
Hello Britt,
would be good to update your version with the Transient Reference Design eventually also the model given on this site. http://www.ti.com/product/LM3671/toolssoftware
Cheers Andy
Andy,
The model on the web is for the fixed 2.5V version of the device. It is documented in the TINA-TI reference design. We should probably add the adjustible version to the product folder. This is a case where there are many fixed voltage versions and the adjustable voltage version in the same product folder.
You can also simulate the device in the WEBENCH® Power Designer for all of the fixed voltage versions as well as voltage values where there is not a fixed voltage version.
Britt