Hi I'm trying to develop a voltage regulator that has two different outputs, but i want them to be on the same board. I need one output to be 12v @ 16A and the other one to be 3.3V @ 0.5A. I just want to have to different lines coming out of the same regulator to give to my motor controllers instead of having to develop two different voltage regulators. Thank you.