Other Parts Discussed in Thread: OPA2320
Dear Support Team,
my customer is experiencing issues in simulating the spice model downloaded from the website. The errors are displayed in the following. Do you have any suggestion?
Thanks a lot
Nicola
Message (1): Line 53:
C_C4 INN INP 4p TC=0,0
warning -- "TC" is not a recognized element parameter.
Message (2): Line 79:
C_C1 0 N61125 1m TC=0,0
warning -- "TC" is not a recognized element parameter.
Message (3): Line 80:
C_C6 GNDF IN_COMP 18n TC=0,0
warning -- "TC" is not a recognized element parameter.
Message (4): Line 85:
C_C2 INN GNDF 2p TC=0,0
warning -- "TC" is not a recognized element parameter.
Message (5): Line 89:
C_C3 GNDF INP 2p TC=0,0
warning -- "TC" is not a recognized element parameter.
Message (6): Line 92:
.model Dbreak D N=0.001 RS=0.001 T_ABS=27
info -- The "T_ABS" parameter is being added to the device "D_D1" as "TEMP".
Message (7): Line 102:
.MODEL DVN D KF={PWR(FLW,0.5)/1E11} IS=1.0E-16
error -- Unsuppported expression form "{PWR(FLW,0.5)/1E11}". This card will be turned into a comment.
Message (8): Line 180:
EMETER VIMON GNDF VALUE = {I(VSENSE)*GAIN}
info -- Voltage controlled voltage source is converted to an arbitrary voltage source.
Message (9): Line 298:
.MODEL DVNF D KF={PWR(FLWF,0.5)/1E11} IS=1.0E-16
error -- Unsuppported expression form "{PWR(FLWF,0.5)/1E11}". This card will be turned into a comment.
*********** END OF BEGIN OF ERRORS/INFO/WARNINGS *************