Other Parts Discussed in Thread: TPS54060, TPS54040
Hello!
I have an issue with TPS54060DGQ. I'm using component values from the SwitcherPro designer. I didn't use the exact suggested diode but similar.
I followed the layout suggestions.
I am hand soldering with an iron. I have one board which seems to be working but I have had 4 boards fail and the part that fails is the TOS54060. It just gets really hot and smokes.
There is good continuity from PowerPad to GND pin. There is only one large via in the PowerPad to the GND plane and one large via just to the top of the PowerPad to the GND plane.
Any thoughts?
Thanks!
Sophi