Other Parts Discussed in Thread: TPS61045, TPS61040, TPS61041
HI,
I have tried to run the pspice transient model on orcad 16.6.However when i simulate the circuit it give me this error.
----------------------------------------------------------------------------------------------------------------------------------------------------------
**** 06/23/14 13:11:50 ***** PSpice 16.6.0 (October 2012) ***** ID# 0 ********
** Profile: "SCHEMATIC1-test" [ D:\U of T course material\Summer research-2014\circuit simulation\cadence simulation\charging capac
**** CIRCUIT DESCRIPTION
******************************************************************************
** Creating circuit file "test.cir"
** WARNING: THIS AUTOMATICALLY GENERATED FILE MAY BE OVERWRITTEN BY SUBSEQUENT SIMULATIONS
*Libraries:
* Profile Libraries :
* Local Libraries :
.LIB "../../../charging capacitor-pspicefiles/library/tps61045/release_ti/pspice/tps61045_pspice_trans/tps61045_trans.lib"
.LIB "../../../charging capacitor-pspicefiles/library/mrb0530/mrb0530.lib"
.LIB "../../../charging capacitor-pspicefiles/library/tps73101_pspice_trans/tps73101.lib"
* From [PSPICE NETLIST] section of C:\Users\user\AppData\Roaming\SPB_16.6\cdssetup\OrCAD_PSpice/16.6.0/PSpice.ini file:
.lib "nomd.lib"
*Analysis directives:
.TRAN 0 0.01 0
.OPTIONS ADVCONV
.PROBE64 V(alias(*)) I(alias(*)) W(alias(*)) D(alias(*)) NOISE(alias(*))
.INC "..\SCHEMATIC1.net"
**** INCLUDING SCHEMATIC1.net ****
* source CHARGING CAPACITOR
C_C7 0 VOUT 1uF TC=0,0
C_C4 0 N10016 100nF TC=0,0
R_R3 N10094 N10160 125k TC=0,0
R_R5 N10160 VOUT 1.42M TC=0,0
R_R4 0 N10160 200k TC=0,0
C_C6 N10160 VOUT 22pF TC=0,0
L_L1 N10046 N10062 10uH
X_U7 N10062 VOUT D_D1
C_C5 0 N10046 4.7uF TC=0,0
X_U8 N10046 0 N10094 N10160 N10062 N10016 0 0 TPS61045_TRANS
V_V3 N10016 0 5Vdc
**** RESUMING test.cir ****
.END
--$
ERROR(ORPSIM-16318): Missing or invalid expression
ERROR(ORPSIM-15108): Subcircuit $ used by X_U8.X_u_S1 is undefined
----------------------------------------------------------------------------------------------------------------------------------------------------------
Is there anything run with how I run it or is it the model's problem? If it is the model's problem , what should I do to fix the error. Thanks for your help
I just want to note that I also tried the tps61045-trsn.DSN file and the model insider still provide me with the same error.