This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

really poor transient simulations for an LM3150 design

I posted this in another forum but it was suggested I put it here instead:

-----------

Hi,

I did a design in webench using the LM3150 and pretty much set it up the way it was advised.  When I run the Vin and Iload transient simulations the results are terrible.  i.e. 1/2V shift in the output with a 1V input step, accompanied by oscillations.

Can someone evaluate if this is a valid simulation response for me?

I suppose I need an email to share the design to.

Thanks.