This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Speaker Array Designer

Other Parts Discussed in Thread: LM48901, LM48903

Hi,

I am trying to use this tool http://webench.ti.com/sawa/#main ; however, I cannot open the dat file that it produces.

I am wondering if you could point me to the application that would allow me to open it. 

Thanks!

Juan Serrano

  • Hi Juan,

    The Speaker Array Designer online tools were designed to be used with two speaker array chips, LM48901 and LM48903. Are you using either of these devices?

    These devices are now under limited support by TI (they do not even have product pages anymore). The .dat file output of the Speaker Array Designer is a coefficients file which can be loaded onto the LM48901 and LM48903 chips on their evaluation modules.

    Kris