Other Parts Discussed in Thread: TINA-TI
Hello
Does TINA-TI support BSIM3V3 MOSFET models? I try to import such a model but get an error message that it is not supported. Thanks.
Regards
Silvio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TINA-TI
Hello
Does TINA-TI support BSIM3V3 MOSFET models? I try to import such a model but get an error message that it is not supported. Thanks.
Regards
Silvio
Silvio,
There are several versions of the BSIM3v3 model. TINA-TI supports the Compact Model Council approved version of BSIM3v3.3. The BSIM3v3.2 version (supported in PSpice as Level 6) is not supported in TINA-TI. I believe that the other model versions (higher than 3v3.3) can also be used in TINA-TI. If you could provide the model, we could check to see if it is supported.
There are several different parameters wit the BSIM3v3 models and some may not be supported, but the model will still run in TINA-TI if the parameters are commented out.
Britt
Hi Britt
Thanks for quick reply. I have attached the model I try to include in TINA-TI.
Regards
Silvio
Silvio,
Try this one.
The Level for BSIM3v3 in TINA-TI is 7. I changed it in the model file and it imported correctly.
Britt
Hi Britt
I have imported the macro file but fail to simulate even a simple circuit due to convergence problems. 4784.2SK4177_Test.TSC
Not sure wether import into TINA-TI is the problem or the model itself.
Regards
Silvio
Silvio,
I will take a look at the circuit. I, too, am not sure if the model or TINA-TI is the issue at this point. I'll post back to this thread when I get more information.
Britt
Silvio,
The error is caused by the version of the BSIM3v3 model. TINA-TI supports BSIM3v3.1 which does not have CAPMOD 3 as an option. You can change the value of CAPMOD to 2 and the device will function, however, the capacitance equations will be different than the equations that were used when the model was created. You can find the differences between CAPMOD 2 and 3 with a quick google search. If any of the CAPMOD 3 features are key to your use of the model, you may not get the proper results.
I am attaching the .TSC file with the modified model in it.
Britt
Hi Britt
Thanks for your help. I can confirm that when changing to CPMOD=2 it is possible to simulate simple circuits. However, the real target circuit, which includes a cascode configuration, does still fail with convergence problem.
Nevertheless, I will stop here to investigate this in more detail as this MOSFET was only one possible candidate and other MOSFET models are working good. I will later check this MOSFET on a hardware prototype, which seems to be easier than getting this model to work reliabily.
Regards
Silvio