This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FLYBACK UCC3809 OrCAD/PSpice convergence problem

hello

i'm tring to simulate flyback with UCCx809-2 controler and i have
some problems with simulation. i have convergence problems. i'm using OrCad 16.3:

These voltages failed to converge:

V(COLLECTOR) = 5.000V \ 4.147V
V(N50537) = 5.069V \ 4.623V
V(X_U1.clk) = 4.995V \ 4.549V
V(X_U1.13) = 4.545V \ 4.098V
V(X_U1.7) = 5.000V \ 4.554V
V(X_U1.ref5vint) = 5.000V \ 4.554V
V(X_U1.20) = 5.000V \ 4.147V
V(X_U1.24) = -10.00V \ -9.107V
V(X_U1.PWMq) = 5.000V \ 4.554V
V(X_U1.21) = 5.000V \ 4.147V
V(X_U1.22) = -10.00V \ -9.107V
V(X_U2.5) = 5.000V \ 4.147V
V(X_U2.6) = 192.37mV \ 191.82mV
V(NC) = 192.37mV \ 191.82mV
V(X_U2.7) = 1.039V \ 867.82mV
V(X_U3.8) = 1.643V \ 1.647V
V(X_U1.X1.Qint) = -343.51mV \ -320.94mV
V(X_U1.X1.Qqq) = -312.84mV \ -292.29mV
V(X_U1.X1.Qqqd1) = 2.498V \ 2.275V
V(X_U1.X2.Qint) = 4.897V \ 4.875V
V(X_U1.X2.Qqq) = 4.460V \ 4.440V
V(X_U1.X2.Qqqd1) = 5.000V \ 4.554V
V(X_U1.X_U1234.INP2) = 6.375V \ 5.806V
V(X_U1.X_U1234.1) = 5.000V \ 4.554V
V(X_U1.UVLO_INT) = 5.000V \ 4.554V
V(X_U1.X2.X3.YINT) = 5.000V \ 4.554V

These supply currents failed to converge:

I(X_U1.EBRegate) = -33.34uA \ -27.65uA
I(X_U1.X1.X3.E_ABMGATE) = 2.498A \ 2.275A
I(V_V1) = -10.00GA \ -10.00GA
I(X_U1.VMRef) = -33.34uA \ -27.65uA
I(X_U3.V4) = -1.014uA \ -924.24nA
I(X_U1.X2.V1) = 5.000A \ 4.554A

Almost all errors refers to UCCx809-2 controler (X_U1).
When i set autoconvergence i have less errors:


These voltages failed to converge:

V(X_U1.13) = 4.500V \ -500.00mV
V(X_U1.7) = 5.000V \ 0V
V(X_U1.ref5vint) = 5.000V \ 0V
V(X_U1.X1.Qbr) = 0V \ 5.000V
V(X_U1.X2.Qbr) = 0V \ 5.000V
V(X_U1.X_U1234.1) = 93.13nV \ 10.43mV
V(X_U1.UVLO_INT) = 5.000V \ 559.68KV
V(X_U1.X_U2345.YINT) = 0V \ 5.000V

These supply currents failed to converge:

I(X_U1.EBref) = -485.29uA \ -7.000uA
I(X_U1.X1.EQb) = 0A \ -5.000A
I(X_U1.X2.EQb) = 0A \ -5.000A
I(X_U1.X_U1234.EOUT) = -5.000A \ -559.68KA
I(X_U1.X_U2345.E_ABMGATE) = 0A \ -5.000A
I(V_V1) = -10.00GA \ -10.00GA
I(X_U1.VSS) = 478.29uA \ -693.32fA

These devices failed to converge:
X_U1.DSS X_U1.DVdd X_U1.X1.GQ X_U1.MBF X_U1.MTF

ERROR -- Convergence problem in transient analysis at Time = 11.64E-18
Time step = 11.64E-18, minimum allowable step size = 40.00E-18

These voltages failed to converge:

V(OUT) = 123.51V \ 144.07V
V(X_U1.24) = 113.51V \ 134.07V

These supply currents failed to converge:

I(X_U1.EBref) = -7.000uA \ -485.29uA
I(X_U1.EBout) = -1.135A \ -1.341A
I(V_V1) = -10.00GA \ -10.00GA
I(X_U1.VSS) = 4.510pA \ 478.29uA

These devices failed to converge:
X_U1.DVdd X_U1.MBF X_U1.MTF

Now errors refers only to controler.

When i simulate independently the power section and feedback loop with the same
values i don't have any problems

What should i do to run this simulation?

  • Lukasz,

    Convergence problems can generally be solved by loosening the simulation parameters. Are you getting DC convergence error (at time t=0 in the transient simulation) or transient convergence errors (at time > 0 in the transient simulation)? In either case, since voltages and currents are affected, you can try increasing VNTOL (for voltage) and ABSTOL (for current). If it is a DC convergence error, try increasing ITL1, if it is a transient convergence error, try increasing ITL4.

    Best regards,