Hi,
I am conducting a current consumption analysis of a circuit aiming to drive a piezoelectric actuator.
My simulation is working fine.
I need to record the current at different points of my circuit. To do so, I have place ammeters at each point I need to have a current measurement.
After running a transient analysis, I record the RMS and Absolute Average values for each current curves by selecting the curve > clicking Process > Averages...
I would like to know if it is possible to modify the precision of the value because when the RMS current is lower than 1mA, the value is very precised :
1.138*10-5 A
but as soon as the RMS current is higher than 1mA, the value shown is :
0.001 A which is a round value.
Does someone knows how to prevent the Tina to round the value like that? If not, I am interested in any way to get the average and RMS values of a current.
I thank you in advance
Valentin