This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps40042 analysis Vout wrong

Other Parts Discussed in Thread: TPS40042

A customer reported in switcherpro(and I verified) that on the analysis - output1 - output voltage min/max for the following design, both are filled in with -1.000, incorrectly.  Why?

 

Design specifies 40042 with Vin min = 3.0V, Vin max = 3.6V, Iout max = 13A, Vout - 1.05V

 

thanks, jack