Hello,
I used Webench to create a schematic for the LM3150 DC-DC Converter.
Input: 26~32 V; output: 24 V /8 Ampere;
I have not changed the component types, manufacturer.
(1)I found the temperature of LM3150 is about 80°C.
Is the temperature high when LM3150 works ?
(2) The output voltage drop below 24 V (about 15V).
Is there any suggestion for this case?