This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Webench simulation / LM20343



Hi Team,
 
I'd like to ask about LM20343 webech simulation.
Our customer is going to use LM20343 on the following condition.
◇Vin(typ)=20.5V,Vout=16V,Iout=2.5A
 
I was able to simulate in webench.
 
Does this simulation result use max duty cycle typ(80%)?
Is it the condition that is feasible with a real board?
 
Customer feel uneasy.  
 
 
 
Best Regards,
Yusuke / Japan Disty
  • Hi Yusuke,

    According to the operating values in your design report, the duty cycle is 79.897%. The design should run fine on a well-designed board.

    Let me look more into this for you, and I can see if I can provide you with some PCB files to get your customer started with a highly functional PCB design.

    If you have any other questions please feel free to contact me.

     

    Regards,

    Andres Preciado

    Webench Applications Engineer

    669-721-7680