This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Capacitor Tolerance Values In Webench

Expert 2071 points

In Webench, the capacitor tolerances appear to be off by a factor of 100.  Is this a matter of incorrectly displaying the tolerance as a percentage?  Or is the simulation using an incorrect tolerance value?  Are the tolerances even used in the simulation?  Here is a screenshot of an example of what I'm talking about:


Thanks,

Greg