This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello there
One of my customer requested Phase margin simualtion with TPS82740A. I tried to find our web, however there is no average reference design file.
If you don't mind, could you share the data? or simulate for 2.5V with 100mA.
Thank you.
Hi Jacob,
Since this is based on DCS Topology which is hysteretic, an average model is not applicable. Since this is a module with internal L and C, there is not much to change anyway for the customer. If you do want to test the stability, you could create a design for TPS82740A in WEBENCH and run Load Transient simulations to see the response.
Thanks,